Language Element toolbar

Language Element toolbar

LanguageElementToolbar_v31
The
Language Element
toolbar is a tabbed toolbar that shows the instruction set in tabbed categories. Select a category tab to display that instruction category in the instruction toolbar. Tooltips on the toolbar indicate the intended use for each tool. Move the cursor over the icon and the tooltip appears.
This toolbar also has a scrollbars for the tabbed instruction groups, and another scrollbar for the instructions within a group. Click these scrollbars to move through the groups or instructions.
TIP:
If a project uses a controller that does not have a serial port, any ASCII Serial Port instructions placed in the Favorites toolbar (Ladder Diagram or Structured Text) are still visible, but are disabled (grayed out).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal