Accept Instruction Modifications

Accept Instruction Modifications

Editing the instruction’s Mnemonic field changes the instruction type. When this change (Morphing) takes place, the operands remain in the same order (fore example, Operand 1 of original is Operand 1 of Morphed).
Examples (in ASCII):
Original Instruction
Morph To
New Instruction
TON Op1 Op2
XIC
XIC Op1
XIC Op1
TON
TON Op1 ?
TON ? OP2
XIC
XIC ?
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal