Split the viewing window
When you are working with projects in the Logix Designer application, you can make the display work to your advantage. Using the splitter bar, you can split the Routine View and show two separate panes of the view. When a routine is initially displayed, the upper pane is not shown.
To: | Do this: |
Move the splitter bar | Drag the bar up/down (or select Split from the Window menu) to resize the upper and lower panes. |
Switch between different panes of a Routine View | Press the F6 key. |
If you use the splitter to close the active pane, all editing operations in the editor will be disabled while the current input focus is for the closed pane.
If you move the splitter to close the active pane, the Ladder Editor automatically sets the focus to the next pane.
Provide Feedback