Use scroll bars
The scroll bars allow you to view different parts of any display or file that is too large to display in the viewing window. There are two scroll bars: one for horizontal movement, and one for vertical movement.
Scroll bars consist of three elements: the scroll bar itself, the scroll box (or thumb), and an arrow on each end.
To use the scroll bars:
- Click in the scroll bar on either side of the scroll box (between the thumb and the arrow) to move in large increments
- Click either arrow to move in small increments
- Click and drag the scroll box to jump to a desired location
Provide Feedback