Plug-In Manager dialog box
Use this dialog box to view the names, descriptions, versions, and properties of plug-ins installed with the
Logix Designer
application. When you install a plug-in that is compatible with the Logix Designer
application, you use it to add custom properties to a project. The custom properties are stored with the project file and are accessible to the associated plug-in when you open the project in the Logix Designer
application. Custom properties can be downloaded to the controller and are imported and exported with the project.You can also use this dialog box to delete all custom properties stored in the project for a plug-in. When a plug-in is not registered with
Logix Designer
application, removing the custom properties for the plug-in removes the plug-in from the plug-ins list.
TIP:
Top open the
Plug-In Manager
dialog:
- On theToolsmenu, selectPlug-In Manager.
Provide Feedback