- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Backplane modules
When choosing to print a report on a backplane module a backplane may be:
- 1756 Backplane
- Backplane,CompactLogixSystem
- NetLinx Backplane (from 1788-ENBT)
- FFLD Backplane
- Backplane, 1789-Ann/A Virtual Chassis
- ArmorPOINT®chassis (various sizes)
- POINT I/Oin Slot Chassis
- CIP Bus from Ethernet Bridge module
- Isysnet N Slot Chassis (Parker Hannifin)
- XM®(1440 device)
- Any object the Controller Organizer recognizes as a backplaneTIP:Backplane module reports include properties for the communication module in the backplane. All other component reports only display data for the selected component, not its communication modules.
Provide Feedback