- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Save pending edits to execute online command?
Certain commands (Motor/Encoder Test) require saving any pending edits on the current
axis before they can execute. Answering Yes lets you continue with the command sequence;
answering No aborts the command sequence.
The Motor Test command requires you to observe the direction of axis motion when executed
to determine whether the desired positive motion of axis matched the direction of motion
when Motor Test was executed.
Provide Feedback