Lock all License-Protected content

When a routine or an Add-On Instruction is protected by License Source Protection, it should be locked if it is shared outside a trust boundary, such as being emailed over the internet or sent to an end customer. Projects that contain unlocked components are in a less secure state than locked components and should not be distributed.
To lock all license-protected components in a project at once, use the
Lock All
button on the
Security toolbar
.
  1. Apply License Source Protection to the components that you need to protect.
  2. On the
    Security toolbar
    , select the
    Lock All
    button. This button is disabled when there are no components to be locked.
    You can also select, on the main menu,
    Tools > Security > Lock all unlocked content
    .
    TIP: If an error prevents a component from locking, an error message appears. The Logix Designer application still locks other components that can be locked without error.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.