Argument List dialog box - JSR instruction

Argument List dialog box - JSR instruction

Set the arguments for the JSR instruction. The following arguments are available:
  • Routine
    : Select a routine name to use for the subroutine to execute in the list, or type a routine name directly into the box.
    TIP:
    MainRoutine
    ,
    Current Routine
    ,
    and
    Phase State Routine
    are not valid targets as arguments for a JSR instruction, and do not appear in the
    Routine
    list.
  • Input
    and
    Return
    parameters: Select a tag to use for the parameter from the tag browser in the list, or type a tag name directly into the box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal