- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Find a function within a DLL file
An external routine DLL must call a function. Use the
Functions Available
dialog to choose a function from a list.To find a function within a DLL file
- From the Controller Organizer right-click the active routine and then chooseProperties.
- Click theConfigurationtab, and then click theBrowse
button.
- From the list of available functions, choose the function that the external routine calls.
- SelectOKto close theFunctions Availabledialog.
Provide Feedback