Change the order of program execution

Programs execute in the order they appear underneath a task in the Controller Organizer.
To change the order of program execution:
  1. From the Controller Organizer right-click the task in which to reorder the programs, and choose
    Properties
    .
    The
    Task Properties
    dialog appears.
  2. Click the
    Program/Phase Schedule
    tab.
  3. Select the program to reorder in the
    Scheduled
    list.
  4. Click the
    up arrow
    to move the program up one place.
  5. Click the
    down arrow
    to move the program down one place.
  6. Click
    OK
    to reorder the programs.
    The programs now appear in the new order under the task in the Controller Organizer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.