New Component toolbar

Use this toolbar to create a new project component.
NewComponentToolbar_v31
This toolbar gives you a shortcut to the new component dialog boxes in the Controller Organizer and the Logical Organizer. If a button is disabled, that function is not available in the current organizer, or not available for the currently selected item.
  • New Routine
  • New Equipment Phase State Routine
  • New Tag
  • New Module/Select Module Type
  • New Program
  • New Equipment Phase
  • New Equipment Sequence
  • New Folder (Logical Organizer only)
  • New Task
  • New Data Type
  • New Trend
  • New Add-On Instruction
Tooltips on the toolbar indicate the intended use of each tool. Move your cursor over the icon and the tooltip appears.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.