Path bar

Path bar

The Path Bar indicates the current communications path.
PathBar_v31
Selecting the RecentPathIcon_v31 button on the right side of the path bar opens the
Select Recent Path
dialog, from which you can choose a communications path from a recent project.
Selecting the WhoActiveIcon_v31 button opens the
Who Active
dialog , from which you can select a target controller, or update your communications path.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal