- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Security toolbar
Use the
Security
toolbar to: - Lock or unlock individual license-protected components in a project.
- Lock all license-protected components in a project.
- Open theSource Protection Configurationdialog box.
If the toolbar is not visible, on the main menu click
View > Toolbars
and select Security
to display it.The following table describes the buttons on the toolbar.
Button | Description |
---|---|
![]() | Opens the Source Protection Configuration dialog box. |
![]() | Locks all license-protected content in the project that is not locked. Click this button before sending a project across a trust boundary. For example, do not email an unlocked project over the Internet without either locking license-protected content, or encrypting the project file using a method such as a password protected zip file or Pretty Good Privacy (PGP). This button is enabled only when a project contains unlocked content, and the controller supports Execution Protection and component locking. |
![]() | Locks the selected component. |
![]() | Unlocks the selected component. |
Provide Feedback