No Operation (NOP)

No Operation (NOP)

The NOP instruction functions as a placeholder.
You can place the NOP instruction anywhere on a rung. When enabled the NOP instruction performs no operation. When disabled, the NOP instruction performs no operation.
Available Languages
Ladder Diagram
Ladder Diagram_No Operation (NOP)_v1
Operands
Ladder Diagram
None
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Common Attributes for operand-related faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
N/A
Rung-condition-in is false
N/A
Rung-condition-in is true
N/A
Postscan
N/A
Examples
Ladder Diagram
FTStudio-NOP-LD-EX-V1
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal