Navigation
Navigate the FactoryTalk Hub
Home
page using the different controls to provide you the services and tools you want.You can use the main toolbar to perform these tasks:
- Use theHub Menuto move between the different services included in your organization’s entitlements. This menu also contains hub management tools if you are an owner or admin for the organization.
- Click the Rockwell Automation logo to go to the Rockwell Automation website if you want to view additional product information.
- TheNotificationsbell icon alerts you to any new information since the last time you signed on. Click theNotificationsicon to review the notifications list and respond to alerts. For more information, see Notifications.
- TheHelpquestion mark icon provides you with different forms of help. You can review the release notes, getting started information, and help topics. There are also links that you can use to contact support, provide feedback, or view legal information.
- Click theOrganizationname to switch between FactoryTalk Hub organizations. For example, if you are a member of both a system integrator and a solution provider organization.
- Click yourProfileicon to updateAccount SettingsorLogoutof FactoryTalk Hub.
Portal Menu Features
The portal menu is divided into two sections. Hub Manager and Organization.
- Hub Manager Menu
If you are an administrator for your organization, you can access
Hub Management Features
from the Portal Menu
. The Hub Manager
section lets you Manage User Access
, View Entitlements
, Send Invites
, and Approve Users
.- Organization Menu
The
Organization Menu
gives you options to Create Organizations
, Edit Organizations
, and Join Organizations
. It provides a link to check your Universal Credits Balance.Additional information
If there is a term used in FactoryTalk Hub you aren’t familiar with, check the Glossary for a definition. If FactoryTalk Hub is not operating as expected, contact Support resources.
Provide Feedback