Develop an interface that visualizes a periodic task
This interface visualizes a long-running task.
TIP:
You can download a sample project from:
ExampleApplication-PeriodicTaskVisualization.zipPrerequisites
TIP:
Do not set the project title to
PeriodicTask
. This is a reserved namespace.- To develop the project
- Save the project.
In
FactoryTalk Optix Studio
, select to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.Provide Feedback