Add a polygon pen

Add a polygon pen

Add a polygon pen to visualize the distance between values of an array variable.
  1. In
    Project view
    , select or create an array variable of the
    Number
    data type.
    For more information, see Variables.
    For example, create a variable of the
    Number[2,3]
    data type.
  2. In
    Project view
    , select or create an
    XYChart
    object.
  3. In
    Properties
    , next to
    Pens
    , select
    Add
    Add
    and select
    Polygon line pen
    .
  4. Create a dynamic link between
    Point array
    and the array variable.
    For more information about dynamic links, see Create dynamic links.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal