Installation and updates

Installation and updates

You can install
FactoryTalk Optix Studio
or access it from the supported web browser through
FactoryTalk Hub
.

FactoryTalk Optix Runtime

Runtime software that is deployed to
FactoryTalk Optix Application
client systems. The software required for client systems varies depending on the operating system. On
Rockwell Automation
client systems, the required software is preinstalled.

FactoryTalk Optix Application Update Service

If necessary,
FactoryTalk Optix Studio
automatically updates the
FactoryTalk Optix Application Update Service
when deploying an
FactoryTalk Optix Application
to the client system. Once the update completes, the application deployment continues.
IMPORTANT: On Microsoft Windows client systems, you must upgrade the
FactoryTalk Optix Application Update Service
manually by updating
FactoryTalk Optix Runtime
Tools installation. See Install FactoryTalk Optix Runtime.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal