Configure an alarm grid

Configure an alarm grid

Add a table that displays alarms status in real time.
  1. From the toolbar, select
    Template Libraries
    Template Libraries
    .
  2. In , search for
    Alarm Grid
    .
  3. Under
    Components
    , drag
    Alarm Grid
    onto
    Page2 (type)
    in
    Project view
    .
    AlarmGrid1
    appears under
    Page2 (type)
    .
  4. Select
    Close
    .
  5. In
    Project view
    , select
    AlarmGrid1
    .
  6. In
    Properties
    , set
    Horizontal alignment
    to
    Stretch
    .
    The object adjusts its width to the container at runtime.
AlarmGrid1 in Page2
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal