FactoryTalk Optix Studio web version

FactoryTalk Optix Studio web version

You can use
FactoryTalk Optix Studio
in a web browser through
FactoryTalk Hub
.

Editor features support

FactoryTalk Optix Studio web version
supports all
FactoryTalk Optix Studio desktop version
features except for:
  • Save logs from the
    Output
    tabs.
  • Edit NetLogic files.
  • Open
    FactoryTalk Optix Studio
    Help Center.
  • Display paths in logs in the
    Output
    tabs.
  • Draw lines, polylines, rectangles, and ellipses in the editor.
  • Add and use custom fonts.
  • Add files and images by dragging and dropping them into
    FactoryTalk Optix Studio web version
    .
  • Restart the application at runtime by using the
    Commands
    Core commands
    Restart
    method.

Emulator features support

FactoryTalk Optix Studio web version
emulator supports all features of
FactoryTalk Optix Studio desktop version
emulator except for:
  • Display animations in the runtime emulator.
  • Control the
    WebBrowser
    object in the runtime emulator.
  • Control the
    PDFViewer
    object in the runtime emulator.
  • Control the
    Video
    object in the runtime emulator.
  • Control the
    Window
    object in the runtime emulator.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal