Add an event to an object from another object

Add an event to an object by adding an event from another object. This prevents you from having to recreate the same event for different objects.
  1. In
    Project view
    , select the object to which you want to add the event.
  2. In
    Properties
    after
    Events
    , select
    Add
    external
    event
    .
  3. Navigate to the object that has the event you want to add to the current object, select the event, and then click
    Select
    .
  4. To associate a method with the event, after the event, select
    Add net method
    and select the desired method.
  5. In the selection window, navigate to and select the method to add:
    • Global method. Expand the
      Commands
      node and expand the method node to select a method.
    • Local node. Expand the node of the object to select a method.
  6. Click
    Select
    .
  7. (optional) If the method requires arguments, expand the method and set the arguments.
  8. (optional) Associate any additional methods with the event.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal