- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Graphic and layout objects
Use graphic and layout objects to create a
FactoryTalk Optix Application
user interface.To create the user interface, design:
- Structure and hierarchy of graphic objects
- Position of graphic objects
- Navigation mechanisms
TIP:
The user interface design is independent of the device and the presentation technology used to display the application at runtime.
Provide Feedback