Time zones for alarm events

Time zones for alarm events

At runtime, the
Data grid
object of the
Alarm grid
and
Alarm log grid
objects display the local time of events in the
Timestamp
column:
Object
Timestamp
Alarm grid
Set a dynamic link in the
Time
property.
Alarm history grid
Set a dynamic link in the
Time
property with a node pointer.
In projects that support remote sessions, devices with different local time settings can display different time zones in the widgets. The timestamp of the widget displays in the local time zone of the device, even when events occur in different time zones. In the
Timestamp
column of the
Alarm grid
or
Alarm history grid
, set a converter of type
Expression evaluator
with the sum of the properties
{Item}Time
and
{Session}TimeZoneOffset
. See  View alarms in remote local time zone.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal