- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Change user properties
Change the properties of a user to modify the domain, password, location, and language for that user.
- InProject view, expandSecurity.
- ExpandUsers.
- Select a user.
- InProperties, change:
- Name. Name of the user.
- Password. Password that the user must provide to log in to the application.
- LocaleIds. Location of the user. The default is en-US.
- Languages. Language configured for the user. The default language is the default language of the location of the user.
- Measurement system. The measurement system used to display data to the user:
- International system of units
- US customary measurement system
- British imperial units
- Domain. Identifies the localWindows®user account for a domain-linked user account.
- SelectSave.
Provide Feedback