View changes to a project

View changes to a project

View the committed changes of the open project by viewing the project history.
In
View history
, represents a change that is committed to the local repository and represents a change that is pushed to the remote repository. If you are not using version control on your computer, Configure version control to view project history in
FactoryTalk Optix Studio
.
  1. In the main toolbar of the open project, select
    View History
    .
  2. In
    View history
    , select to select a commit. The changes in the commit appear highlighted. If the project is new, all content for the project is highlighted.
  3. Expand a highlighted object to view the changes in the object.
    TIP: Values that change in an object are crossed out and an arrow points to the new value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal