Create a button that shuts down the host system

Create a button that shuts down the host system

Add a button that shuts down the host operating system on which the
FactoryTalk Optix Application
runs.
IMPORTANT:
Pressing
Shut down system
immediately shuts down the host operating system
on which the
FactoryTalk Optix Application
runs.
For example, if you run the
FactoryTalk Optix Application
on an emulator target, pressing
Shut down system
immediately shuts down your Windows system.
  1. In
    Project view
    pane, right-click
    MainWindow (type)
    and select
    New
    Base controls
    Button
    .
  2. Hover-over the button, select
    Edit
    , and enter
    ShutDownSystemButton
    .
  3. In
    Properties
    , set
    Text
    to
    SHUT DOWN HOST SYSTEM
    .
  4. In
    Events
    , next to
    MouseClick event
    , select
    Add
    and select
    ProjectName
    NetLogic
    ShutDownSystemNetLogic
    SystemShutDown
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.