Variable Owner: direct access to the NetLogic parent object

Variable Owner: direct access to the NetLogic parent object

Each NetLogic displays the
Owner
variable, which represents the parent node of the same NetLogic. It is useful for directly accessing this node.

Example

This example shows the value of the NetLogic parent node
BrowseName
assigned to the C#
name
string variable.
string name = Owner.BrowseName;
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.