Change the user authentication mode
Change the default user authentication mode for the project to allow local
Windows®
users and Active Directory users to log on to the FactoryTalk Optix Application
.
IMPORTANT:
If you use the Active Directory user authentication mode, Active Directory queries the groups associated with the users are and maps with the existing groups in
Project view
. For example:- A user belongs to a group in the model.
- The same group exists in Active Directory.
- In Active Directory, the user does not belong to the group.
- The user is removed from the group in the model.
- InProject viewpane, select the project node.
- InProperties, inAuthentication mode, select the authentication type that allows specific users to log on:
- Model only. Users you create inFactoryTalk Optix Studio.
- Local only. LocalWindowsusers.
- Domain only. Active Directory users.
- Domain and local. Active Directory and localWindowsusers.
- Any. Users of any type.
- Select.Save
Provide Feedback