Key-value converter

Key-value converter

Convert the value of the source to its corresponding parent value based on a table of key-value pairs. The key-value converter converts heterogeneous data, such as a color to value.

Key-value editor

You can open the key-value editor by selecting
Edit
next to the key-value converter in advanced dynamic link editor.
Item
Name
Description
1
Converter path
The path to the converter.
2
Add
Adds a key-value table row.
3
Delete
Deletes the selected key-value table row.
4
Data type
Indicates the data type of keys or values. Select to choose a different data type.
5
Key
A converter key (source value).
6
Value
A value that corresponds with the key in the same row (output value).
TIP: The value in the first row is the default value. If the source value does not correspond with any converter key, the converter returns the default value.

Properties

Property
Description
Mode
The direction of the dynamic link:
  • Read from the source node to the parent.
  • Write from the parent to the source node.
  • Read from the source node to the parent and write from the parent to the source node.

Source

A variable with a value corresponding to a key.

Output

The value associated with the key in the map.

Example

Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal