- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Create an embedded database
Create an SQLite database embedded in your project. Typically, embedded databases manage data supporting other objects within the
FTOptixApplication
.- InProject view, right-clickDataStoresand selectEmbedded database.
- (optional) InProperties, inFilename, enter a custom name for the database file.
- SetIn memoryto either:
- True. Makes the database non-persistent. The stored data is removed when you restart theFactoryTalk Optix Application.
- False. Makes the database persistent. The stored data is kept when you restart theFactoryTalk Optix Application.
(optional) Configure the database structure. See Configure a database table.
database
Provide Feedback