Resize an object

Drag to resize an object or specify values in object properties.
Prerequisites
To resize an object, the alignment of the object must be left, top, or bottom. If the object alignment on the X-axis or Y-axis is
Adjust
, the object sizes dynamically according to the size of the container. You cannot scale the size of an object that is inside a container with respect to the size of the container.
TIP: The size of the
Window
object defines the size of the entire user interface. It can be set using the
Width
and
Height
properties or it can be automatically set equal to the size of the screen on which the interface is displayed at runtime using the
Full Screen
property.
  • To resize an object
  • In the editor, drag a sizing handle on the object.
  • In
    Project view
    , select an object and in
    Properties
    change:
    • Height
      . Enter the value for the height of the object.
    • Width
      . Enter the value for the width of the object.
    TIP: If you delete either the
    Height
    or
    Width
    value, the object uses the
    Auto
    setting. Text determine the size of the object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.