Switch
Sets and displays a Boolean value.
Use case
Enable or disable functions or features within a
FactoryTalk Optix Application
. For example, toggle a graph that visualizes data.Example
Disabled switch with optional text
![Animated graphic showing a sliding switch control toggling from ON to OFF](/content/dam/dita/en/factorytalk-optix/current/_images/ref_switch_ex.png/_jcr_content/renditions/original)
Enabled switch with optional text
![Animated graphic showing a sliding switch control toggling from ON to OFF](/content/dam/dita/en/factorytalk-optix/current/_images/ref_switch_ex2.png/_jcr_content/renditions/original)
Provide Feedback