- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Navigation panel
Panel that contains other panels and automatically organizes panels into tabs that you can navigate.
Use case
Provide end users with a convenient way to navigate between different application panels.
Example
Navigation panel with four tabs

Navigation panel properties: Panels (tabs)

Provide Feedback