- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Import files
You can configure your project to use custom files such as fonts to use in your
FactoryTalk Optix Application
.- In the main toolbar, select.Browse project files
- InProject Files, select.Import file(s)
- Navigate to and select the file to import and then selectOpen.
- CloseProject Files.
Provide Feedback