Duplicate a target device

Duplicate a target device

Duplicate a target device to configure another similar target device.
  1. From the main toolbar, next to
    Run
    , select the target dropdown menu.
  2. (optional) In
    Target device settings
    , to display only the active remote target devices, toggle
    Active remote devices
    .
    TIP: Refresh remote target devices by selecting
    Refresh
    .
  3. Select a target device.
  4. Select
    Duplicate
    .
Configure the duplicated target device properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.