- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Add a variable value change event
Add and configure a variable value change event to display a dialog box when a variable value changes.
TIP:
Instead of using a change event, you can also configure a transition event. For more information about events, see Events.
- InProject view, selectMainWindow (type).
- InEvents, selectand select
- Next toVariable1Changed/VariableValueChangedEvent, selectand select .
- Under, create a dynamic link betweenDialogand .
Provide Feedback