Create a button that shuts down the host system

Create a button that shuts down the host system

Add a button that shuts down the host operating system on which the
FactoryTalk Optix Application
runs.
IMPORTANT: Pressing
Shut down system
immediately shuts down the host operating system
on which the
FactoryTalk Optix Application
runs.
  1. In
    Project view
    pane, right-click
    MainWindow (type)
    and select
    New
    Base controls
    Button
    .
  2. Hover-over the button, select
    Edit
    , and enter
    ShutDownSystemButton
    .
  3. In
    Properties
    , set
    Text
    to
    SHUT DOWN HOST SYSTEM
    .
  4. In
    Events
    , next to
    MouseClick event
    , select
    Add
    and select
    ProjectName
    NetLogic
    ShutDownSystemNetLogic
    SystemShutDown
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal