- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Develop a combo box to pick styles
Create a combo box to choose different application styles. Select a style from the combo box to change the application style at runtime.
Application example


NOTE:
Download a sample project:
StylePicker.zipPrerequisites
- To develop the project
- (optional) Add more graphic objects.For example, add a button and a label. For more information, see Graphic objects.
- Arrange the interface elements.
- Save the project.
Application design example

Select
to run the project using the client
emulator to test your project. To run the project on a remote client, see Add a target device.
Run
Provide Feedback