Input/Output Instructions

Input/Output Instructions

The input/output instructions read or write data to or from the controller or a block of data to or from another module on another network.
Available Instructions
Ladder Diagram and Structured Text
Function Block
Not available
If you want to:
Use this instruction:
Send data to or from another module
MSG
Get controller status information
GSV
Set controller status information
SSV
Send output values to an I/O module or consuming controller at a specific point in your logic
Trigger an event task in another controller
IOT
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal