- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
AuxFeedbackFault
Applies to: Servo Drive axes.
AuxFeedbackFault is a Boolean attribute. It is set when the controller fails to receive feedback from a drive configured for Auxiliary Feedback (in the Motor/Feedback tab of the Axis Properties dialog box). The cause of the fault can be a connection problem, or a hardware problem with either the auxiliary feedback device or its power supply.
AuxFeedbackFault is a recoverable fault.
To recover from an AuxFeedbackFault:
- Fix the underlying problem: either the connection or the device.
- Be sure your program or fault handling routine contains either a:
- Fault Reset (MAFR) instruction, to clear all motion faults for an axis, or
- Shutdown Reset (MASR or MGSR) instruction to return to the axis ready operating state.
The occurrence of an AuxFeedbackFault sets bit #6 of the respective DriveFault or ServoFault attribute, the PhysicalAxisFault attribute and bit #0 of the AxisFault attribute.
Provide Feedback