Equipment Sequence Properties
Use the and
Equipment Sequence
Properties Routine Properties
dialog boxes to set the properties of an Equipment Sequence
. - include generalEquipment SequencePropertiesEquipment Sequenceinformation as well as the configuration of the sequence, the sequencing parameters, and sequence monitoring information.
- Routine Propertiesinclude general routine information and the sheet layout of theEquipment Sequence.
Provide Feedback