On and Off Cycling During Typical Operation
The electromechanical contactor and SSR both switch electricity to a load when signaled to do so. This means that both devices can turn the electrical power to the output load on and off at any point in a sinusoidal wave.
In the United States, electricity is provided at 60 cycles per second, or 60 Hz. When the power supplied to a device does not turn on or off at a zero crossover point in the sinusoidal waveform, voltage spikes occur on the sine wave, and RFI and harmonics are generated. An arc also may occur with this type of random on and off operation.
The contactor and SSR devices operate efficiently (no disturbances when fully turned on or off). However, under normal process operating conditions, the generated harmonics can cause the sine wave provided by the power company to become distorted. This may cause difficulty for the power company’s measurement equipment, making it appear that the measured or required power is greater than the actual power used. This could increase power costs.
An SCR power control module is an electronic semiconductor device designed to regulate the power to an output load efficiently. It can switch the power applied to an output load in milliseconds.
Zero-cross operating mode allows SCRs to function comparably to contactors and SSRs, which operate by turning power fully on and fully off. However, in zero-cross mode, the SCR turns the output on and off at the zero-cross point in the sinusoidal wave, which reduces the potential radio frequency interference (RFI), harmonics and arcing associated with contactors and SSRs. These features make SCR power control module use suitable for electric thermal heating applications, for example.
Assess Your Needs
Assessing the pros and cons of each type of device to determine suitability for a particular application can help optimize thermal control and output in temperature-critical processes.
Advanced Energy, Inc. is a participating Encompass™ Product Partner in the Rockwell Automation PartnerNetwork™. Based in Fort Collins, Colorado, Advanced Energy provides power and control technologies, including power control modules, for high-growth, precision power conversion solutions.
The Journal From Rockwell Automation and Our PartnerNetwork™ is published by Putman Media, Inc.