Loading
Blog
Recent ActivityRecent Activity
5 minute read

5 Key Trends Redefining Smart Manufacturing in 2025

In Conversation with Scott Wooldridge, Regional President, Asia Pacific, Rockwell Automation

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Three people in helmets walking in the plant.

With the APAC smart manufacturing landscape crossing $53 billion

in valuation last year, what lies ahead in 2025? Scott Wooldridge, Rockwell Automation regional president, shares the key trends that will define how we build, move, and innovate. The question is: Are you ready to embrace them?

 

Trend 1: Artificial Intelligence (AI) in Manufacturing Will Become Pervasive and Deeply Use-Case Driven

According to Scott, artificial intelligence (AI) is moving away from being a buzzword to becoming an embedded enabler in manufacturing. One example is AI-driven predictive maintenance, enabling machines to signal potential failures before they happen, reducing unplanned downtime and saving costs. Imagine identifying defects before they cascade into costly recalls. This is a reality powered by smart manufacturing and AI.

Additionally, AI will reimage quality control, which historically, is an end-of-line process, often leading to wasted shifts if defects are discovered late. Today, AI-powered vision systems are transforming this scenario by performing real-time analytics directly on production lines — detecting issues like product tolerances or assembly errors on the fly. The result? Faster resolutions, less waste, and better overall quality.

Real-time feedback loops not only enhance quality but also empower teams to act instantly. In a world where speed and precision dictate success, these systems are indispensable. AI’s ability to learn from historical defects and adjust parameters in real-time ensures a continuously improving production process.

In fact, 85% of respondents in our 2024 State of Manufacturing report

have already invested or plan to invest in AI or ML. Respondents predict that by 2027, artificial intelligence will have made the biggest positive impact on quality and cybersecurity, which is also a key trend for 2025. 

 

Trend 2: Autonomous Mobile Robots and Other Smart Systems Open New Possibilities Beyond Fixed Production Lines

For decades, manufacturing depended on fixed conveyors and predefined production lines. But with autonomous mobile robots (AMRs), the game is changing. “AMRs eliminate the need for rigid infrastructure,” Scott explains. “They can transport raw materials, move products between machines, and adapt to dynamic layouts.”

Whether retrofitting a brownfield plant or designing a greenfield facility, AMRs introduce agility. No longer constrained by static designs, manufacturers can optimize workflows while addressing challenges like labor shortages and fluctuating demand. This flexibility means production environments can evolve as quickly as consumer preferences.

Further, smart manufacturing technologies like independent cart systems allow manufacturers to adapt swiftly. These systems replace fixed conveyors with magnetic rails, enabling faster throughput and reduced floor space. Similarly, AMRs equipped with advanced navigation systems are minimizing human intervention, helping to improve safety, and enabling continuous operations in high-risk environments.

Advanced digital twins and simulation technologies further enhance this flexibility, allowing manufacturers to model scenarios, optimize layouts, and make informed decisions in real-time.

In fact, after the impact of the pandemic, manufacturers today prioritize flexibility in their production. Traditional factories were designed to produce the same widget for years. But in today’s market, demand can pivot overnight, which is why autonomous actions by smart systems are so important. However, a holistic platform is needed to tie these technologies together—which brings us to the next trend.

 

Trend 3: MES Will Emerge as a Key Enabling Technology Linking Smart Manufacturing Components

Manufacturing execution systems (MES) are the glue that binds smart manufacturing components. These systems are the key to consolidating and capitalizing on data generated by smart manufacturing environments, a challenge for over 30%

of manufacturers.

Scott elaborates: “MES platforms integrate ERP systems, automate workflows, and provide real-time analytics on production data. This connectivity ensures manufacturers have actionable insights.”

Cloud-based MES solutions like Rockwell Automation’s Plex platform are gaining traction in APAC. Unlike traditional on-premises systems that can take years to deploy, Plex can be operational across multiple plants in months. This speed and scalability make it a cornerstone for manufacturers aiming to stay competitive in a rapidly evolving landscape.

Additionally, MES platforms facilitate seamless integration with IoT devices, AI systems, and robotics, ensuring a unified ecosystem. With built-in compliance tools, MES also helps manufacturers meet stringent regulatory requirements while maintaining operational efficiency, a capability that will prove essential in an era increasingly marked by sustainability concerns.

Trend 4: Manufacturers Will Seek Partners with Dedicated Cyber Expertise to Protect Their Smart Environments

With greater connectivity comes increased vulnerability. As manufacturers embrace interconnected systems, cybersecurity is a critical concern. In 2024, manufacturing emerged as the no.1 sector hit by cyber-attacks, comprising over 25%

of all incidents worldwide.

Scott highlights the need for specialized expertise: “Cyber risks evolve weekly and addressing them isn’t a weekend project. It requires dedicated teams who understand manufacturing’s unique risks.”

By partnering with security experts, manufacturers can build robust defenses without compromising efficiency. The integration of intrusion detection systems (IDS) and anomaly detection technologies help to ensure that cyber threats are identified and neutralized swiftly, safeguarding both data and operational continuity.

Rockwell Automation’s approach includes embedding encryption and secure protocols into new technologies. This is enabled through integrated OT protection powered by Verve, a vendor-neutral solution for risk management across OT assets.

For older plants, refurbishment paths in 2025 need to enhance resilience. Manufacturers must also recognize that traditional IT tools don’t always translate to operational technology (OT) environments. Therefore, vendor-neutral security solutions rooted in the NIST Cybersecurity Framework that cause minimum disruption to the manufacturing environment are needed.

 

Trend 5: Localized ESG Outcomes in APAC Will Be a Top Reason for Smart Manufacturing Adoption

While Environmental, Social, and Governance (ESG) goals are on every manufacturer’s 2025 agenda, priorities differ across regions, and Asia Pacific is no exception. Differentiated ESG targets are becoming a driver for smart manufacturing adoption in 2025.

“In China, the focus is on reducing carbon footprints due to export regulations. In India, circular economy principles like recycling and refurbishing are key. Meanwhile, Australian miners and heavy industry might prioritize employee safety,” Scott reveals. Smart manufacturing supports these goals by offering interconnected systems that measure and validate performance.

Data collection and processing for ESG is another prominent trend for 2025. As Scott succinctly puts it: “If you can’t measure it, you can’t improve it — and you can’t prove it.”

Large manufacturing companies in most geographies need to have an ESG report and must report on their performance. They need manufacturing execution systems (MES) that can report real-time, accurate data on quality, worker safety and energy use. “Using a MES system can help manufacturers to have a benchmark and improve on it moving forward” Scott adds.

We are witnessing a near-industry-wide adoption of smart manufacturing—currently at 95%

up from 83% in 2023. From adoption of cutting-edge solutions like Gen AI to mature technologies like cloud, manufacturing is undergoing an incredible change.

The question is, are you ready to take the first step toward the future of industrial operations?

 

To benchmark your technology usage, explore best practices and uncover smart manufacturing trends in detail, here is a detailed report on the State of Smart Manufacturing.

Published February 24, 2025


Scott Wooldridge
Scott Wooldridge
President, Asia Pacific, Rockwell Automation
Scott Wooldridge is president for Asia Pacific. Scott leads the execution of the company's strategy to bring the Connected Enterprise to life, combining our technology and domain expertise to deliver positive business outcomes for our customers. Scott works with his regional leadership team to implement the Asia Pacific growth initiatives and organizational development plans to meet our long-term objectives.
Connect:
Subscribe to Rockwell Automation

Receive the latest news, thought leadership and information directly to your inbox.

Subscribe now

You may also be interested in
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
  4. Chevron LeftChevron Left Blogs Chevron RightChevron Right
  5. Chevron LeftChevron Left 5 Key Trends Redefining Smart Manufacturing in 2025 Chevron RightChevron Right