From Fluke Corp.
Productivity is the key to survival in today’s globally competitive environment. When you think about the basic inputs to production — time, labor and materials — optimization usually isn’t an option. You have 24 hours per day, labor is costly, and you don’t have much choice in materials. Thus, every company must use automation to gain more output from the same inputs, or perish.
So, we rely on automation, which in turn relies on clean power. Power quality problems can cause processes and equipment to malfunction or shut down. The consequences can range from excessive energy costs to complete work stoppage. Obviously, power quality is critical.
The interdependence of various systems adds layers of complexity to power quality issues. Your computers are fine, but the network is down, so nobody can book a flight or file an expense report. The process is operating correctly, but the HVAC has shut down and production must stop. Mission-critical systems exist throughout the facility and throughout the enterprise — power quality problems can bring any one of these to a grinding halt at any time. And that will usually be the worst possible time.
Power Quality Problems
Where do power quality problems come from? Most originate inside the facility. They may be due to problems with:
- Installation — improper grounding, improper routing or undersized distribution.
- Operation — equipment operated outside of design parameters.
- Mitigation — improper shielding or lack of power factor correction.
- Maintenance — deteriorated cable insulation or grounding connections.
Even perfectly installed and maintained equipment in a perfectly designed facility can introduce power quality problems as it ages.
Using instruments that measure power quality issues generated by harmonics and unbalance can help determine waste. Those instruments then can quantify the cost of that waste based on the unit cost of power from the utility.
Power quality problems also can originate from outside the facility. We live with the threat of unpredictable outages, voltage sags and power surges. How do you quantify the cost?
Measure Power Quality Costs
Power quality problems make their effects felt in three general areas: downtime, equipment problems and energy costs.
Downtime. To quantify system downtime costs, you need to know two things:
- The revenue per hour your system produces.
- Your production costs.
Also consider the business process. Is it a continuous, fully utilized process (such as a refinery)? Must your product be consumed when produced (such as a power plant)? Can customers switch instantly to an alternative if the product is not available (such as a credit card)? If the answer to any of these questions is yes, then lost revenue is difficult or impossible to recover.
Are you an OEM producer? If you can’t make timely deliveries, your customer may switch to a source that can.