After adopting LOPA, the chemical producer saw the need for a scalable, new safety instrumented system to reduce risks and address other critical plant needs.
With a production history dating back to 1899, PPG’s industrial production plant in Barberton, Ohio, United States, is no stranger to change.
Its products have evolved from raw materials for glass-making operations to the range of specialty chemicals it makes today. Its operations have also completely transformed from manual processes to today’s more automated, distributed control-based operations.
One of the recent changes in the plant was how workers evaluate and mitigate safety risks. Recent adoption of the layers of protection analysis (LOPA) risk-assessment method gives workers a better understanding of the effectiveness of plant safeguards – and has even proven useful in identifying areas where they can further strengthen those safeguards.
Safety risks uncovered
The chloroformate unit is one of the Barberton plant’s smallest process units but one of the plant’s highest safety risks.
Workers at the plant have performed process hazard assessments (PHAs) on the unit for decades in accordance with OSHA’s process safety management standard (29CFR1910.119). With the adoption of LOPA, workers now had to evaluate the safeguards identified in those PHAs to quantify and validate their effectiveness.
“We started by evaluating our current interlocks and looking at the scenarios they might be protecting,” said Matt Kinsinger, senior process control engineer, PPG Industries. “Then we re-evaluated anything that we had already ranked as a high risk in the PHAs to make sure it had adequate protection. This helped us to identify opportunities where the existing control system, instruments and control devices could be improved to meet our acceptable risk level.”
From here, Kinsinger and his team developed requirements for a new safety instrumented system (SIS) in accordance with the ISA-84/IEC-61511 standard. The new SIS would need not only to help reduce risk on the process unit but also address other key plant requirements.
These requirements included:
- Usability: The team wanted an easy-to-use operator interface easily integrated with existing distributed control system (DCS) interfaces.
- Scalability: The SIS system must support new or modified plant equipment.
Expandability: The team wanted to be able to easily add to the SIS or add requirements for higher levels of protection based on future analysis or future PHAs.