Calibration Wizard parameters
Calibration Wizard
includes these parameters:Parameter | Description |
---|---|
Channel | Shows the channel number to which this configuration applies. |
Calibrate | Identifies the channels for calibration. Select the checkbox for the channel that you want to calibrate. |
Calibration Range | Shows the value currently configured for the channel.
|
Calibration Gain | Shows the calibration gain values as reported by the device. |
Calibration Offset | Shows the signed values as reported by the device. |
Calibration Status | Shows the status of the calibration per channel as the calibration occurs. |
Low Reference | Shows the value of the low reference signal for the channel. |
High Reference | Shows the value of the high reference source based on the channel configuration. |
Recorded Reference | Indicates the measured output values. For the multimeter accuracy, see the User Manual. |
Status | Shows the value read during calibration for the enabled channels.
If Status shows Error , perform the corresponding actions as needed:
|
Provide Feedback