View current channel calibration
Use the
Calibration
view to view current channel calibration, including:- Channel number of the devices.
- Calibration range value that is currently configured for the channel.
- Calibration gain values as reported by the device.
- Calibration offset signed values as reported by the device.
- Last successful calibration date.
- Calibration status per channel.
To view current channel calibration
- On the tab for the device, selectCalibration.
- In theCalibrationview, view the current channel calibration.
Provide Feedback