Configure individual input channel properties
Configure the properties of the individual input channel to define the scaling and filtering for that channel.
To configure individual input channel properties
- On the tab for the device, expandChannels, and then select an individual channel.
- In theCh0xview, fill in the parameters and selectOK.
Provide Feedback