Product Level Dashboard

Product Level Dashboard

In this dashboard, the user can view the configured hierarchy elements that are child elements of the Product. Based on your configuration, the respective Region or Site details are displayed in the
Overview
tab as cards.
Select the required
Product
from the hierarchy list and the following tabs are displayed in the dashboard:
  • Overview
  • Assets
NOTE: To change the date or time period, refer to Change Date or Time Period.
Overview
The user can view the status of each element of the hierarchy available under
Product
. For example, Minnesota has associated KPIs of Health Index, Reliability, Throughput, and Alert count. The associated KPIs are configured in the Dashboard Setup and the same KPIs are across the application.
The KPI values are rolled up according to the hierarchy, with Alerts and KPI values originating in each asset and rolling up accordingly. The user can also view the top five underperforming assets. All of these are based on the selected time frame selectable in the top right corner of the dashboard.
Product Overview
NOTE:
Click the [>], [>>] and [<], [<<] paginator icons in the summary to move forward and backward to view the data.
NOTE: To know about the card functionality, refer to Card Functionality.
The user can view the individual KPI graph of the
Top 5 Underperforming Assets
and the graph is displayed for the past 3 months. Hover the mouse over the chart to view the selected KPI value with the corresponding date. The user can also select the required KPI from the KPI drop-down list and the corresponding graph is displayed in the
Past 3 Months
column.
Top 5 Underperforming Assets
NOTE: To customize the top 5 underperforming asset table, refer to Customize Top 5 Underperforming Assets Table.
Click the [] icon on the required
Asset Name
to view the
Asset Hierarchy
details.
Asset Hierarchy Details
Assets
The user can view summaries of the asset classes associated with this point in the hierarchy. Each card represents an Asset Class with rolled-up statuses. By selecting an individual
Asset Class
, the user can filter the list of assets available in the
Asset Details
section. Click on the
Asset Name
to view the corresponding Asset page.
Asset Cards
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal